Configure Columns

Some KPIs matter more to you than others. This preference can change over time. Configure columns under Production, Utilization and Summary tabs within Insights.

Arrange them based on what you want to see first. Learn what each column contains and what relevant data you can glean from it.

The columns available under each tab vary based on the asset tags. Click a category to view the respective column tables.

Additional column details are added with new releases. Return periodically to stay updated.


• VisionLink Productivity currently reports partial dump events only for Load Out and Loader – Load & Haul asset tags.
• Get more complete data of dump events, see if discrepancies exist between assets performing dump events, and identify locations where partial dumps occur.
• This information is available under Source and Destination columns in Production (Insights).

 

Production Columns

Asset & Cycle

(Default selection that can't be deselected)

Asset: The physical piece of machinery in the field identified by unique serial number to perform an intended action.

Cycle: The time interval between starting and ending a task by an asset.

Source

(Default selection that can't be deselected)

• Location where a cycle originates.

• For Load & Cycle- or PerformancePro-subscribed assets, the source will be displayed as Unknown.

Destination

(Default selection that can't be deselected)

Location where a cycle ends.

Make

(Default selection that can't be deselected)

Assigned make code or manufacturer for the asset.

Model

(Default selection that can't be deselected)

Unique model number provided for the asset.

Loaded By

(Default selection that can't be deselected)

Asset ID of the loader that loaded the particular hauler.

Cycle Start Time

• Timestamp of when the cycle started.

• Includes date and time.

Cycle End Time

• Timestamp of when the cycle ended.

• Includes date and time.

Estimated Payload (tons)

• Estimated capacity of the hauler and scraper to move payload in a cycle.

• Target Payload is edited in Configure page of Add Assets when creating sites. 

Measured Payload

• Payload value measured using Caterpillar payload systems for a cycle.

• The system needs to be calibrated for this measurement to function properly.

Total Payload

Best available payload for the cycle stored utilizing either Measured or Estimated Payload. 


• VisionLink Productivity utilizes onboard payload as the primary payload data source. If multiple values are available, the best available value will be utilized. 
• For Hauler - Load and Haul and Scrapers specifically, if there is no onboard payload, the Estimated Payload entered will be utilized. 
• You can enter and modify the Estimated Payload when configuring assets during site creation.

Load Time

Time taken by a loader to load one hauler for a cycle.

Travel Loaded Time

Time taken by hauler to travel from load site to the dump site while it is loaded.

Loaded Stopped Time

The summation of all loaded stopped segments for all the assets in selected asset tag operating in site.

Dump Time

Time taken to dump material in the dump site by a hauler.

Travel Empty Time

Time taken by hauler to travel from dump site to the load site while it is empty.

Empty Stopped Time

Total empty stopped segments for all the assets in selected asset tag operating in site.

Miscellaneous Time

Duration of a cycle that could not be classified, but asset operation was recognized.

Cost/Payload

Cost incurred for moving a payload during a cycle for the asset.

Total Distance

Total distance traveled by an asset for a cycle.

Estimated Volume

• Estimated volume that can be moved by an asset from load zone to dump zone during entire load/haul operation.

• Configured during site creation in Add Assets.

Key On - Engine Off Time

Time during which the key was on but the engine was off. Excessive time attributed to Key On – Engine Off indicates time machine was shut down in the middle of a cycle.

Haul Time

Time taken by a hauler or scraper to complete a haul segment.

Load Distance

Distance traveled by a hauler in the load zone during the load segment in a cycle.

Travel Loaded Distance

Distance traveled by an asset while it is loaded.

Dump Distance

Distance traveled by an asset during a dump segment.

Travel Empty Distance

Distance traveled by an asset while it is empty.

Miscellaneous Distance

Distance traveled by an asset during a cycle that could not be classified, but asset operation was recognized.

Haul Distance

Distance traveled by a hauler or scraper during a haul segment.

Fuel Used

Fuel consumed by an asset for a particular cycle.

Load Latitude

Latitude coordinates of the load location of that cycle.

Load Longitude

Longitude coordinates of the load location of that cycle.

Dump Latitude

Latitude coordinates of the dump location of that cycle.

Dump Longitude

Longitude coordinates of the dump location of that cycle.

Material Name

Material type loaded into a hauler during a cycle by a loader.

Custom Lists

• Currently allows users the flexibility of creating up to four custom Remote Lists for data that are not captured by telematics and other devices.

• Examples include material type, operator name, etc.

• This needs manual input and is available for Loader – Load & Haul and Load Out asset tags.

Transmission Shift Count

• Total number of transmission gear shifts made by a driver.

• It helps analyze the wear and tear incurred during each cycle of Haulers - Load & Haul.

• Available for assets subscribed to Advanced Productivity.

Printer Tickets

• Generated at sites for each load event of individual trucks and will include multiple cycles. It has a unique number and acts a physical record of Load events. It helps keep track of payloads and related trucks offline at the site. They are generated for Loader – Load & Haul and Load Out asset tags.

View Sample (Click outside the image to close)

• It reports Pass Count, Cycle IDs, Payload for each cycle and Total Payload, Truck ID, Material ID, Operator ID and the Date & Time of the ticket. At the bottom it displays the unique Ticket Number. It helps keep detailed records as well as to retrieve them when required.


• A Printer Ticket represents a load event and can include multiple cycles. The Printer Ticket Number is associated only with cycles that fall within the corresponding load start and load end time window. Cycles outside this time range will not display the Printer Ticket Number.

Load Site

Name or ID of the load site.

Pass Count

Count of loader passes in a single hauler cycle (productive and non-productive) reported by Advanced Productivity-capable haulers.

 

Utilization Columns

Asset

(Default selection that can't be deselected)

The physical piece of machinery in the field identified by unique serial number to perform an intended action.

Working State

(Default selection that can't be deselected)

• Utilization cycles created during Asset Moving, Asset Stopped, Engine On or Engine Off.

• These can be broken up into substates depending on the action being performed states.

Asset Start Time

Timestamp of when the asset started the cycle.

Asset End Time

Timestamp of when the asset ended the cycle.

Make

Assigned make code for the asset or the manufacturer.

Model

Unique model number provided for the asset.

Total Duration

Total time taken by the asset to complete the cycle.

Total Fuel Burn

Total fuel consumed during the cycle.

Total Cost

Total cost incurred to complete that cycle.

Idle Cost

Total cost incurred during the idling hours of that cycle.

Idle Fuel Burn

Sum of fuel burned during idling of longer than three minutes (short, medium, long) hours for all assets based on asset type and date range which reports fuel.

Asset Start Latitude

Latitude coordinates of the asset location when it started the cycle.

Asset Start Longitude

Longitude coordinates of the asset location when it started the cycle.

Asset End Latitude

Latitude coordinates of the asset location when it ended the cycle.

Asset End Longitude

Longitude and latitude coordinates of the asset location when it ended the cycle.

Working Duration

Total work time of the asset during the cycle.

 

Summary Columns

Asset [View By]

(Default selection that can't be deselected)

The physical piece of machinery in the field identified by unique serial number to perform an intended action.

Time [View By]

(Default selection that can't be deselected)

Depending on the date range selected, it displays hours or days when the cycles are reported to have occurred.

Make

Assigned make code for the asset or the manufacturer.

Model

Unique model number provided for the asset.

Cycles/Hour

Total cycles ÷ max. runtime of selected asset tag.

Payload/Hour

Total payload for selected asset tag divided by total run time.

Payload/Cycle

Total payload for selected asset tag divided by total number of cycles for selected asset tag.

Total Fuel Burn

Total fuel consumed during the cycle.

Total Cost

Total cost incurred to complete that cycle.

Total Distance

Total distance traveled by an asset for a cycle.

Estimated Payload (tons)

• Estimated capacity of the hauler and scraper to move payload in a cycle.

• Added in Configure page of Add Assets step when creating sites.

Measured Payload

Payload value measured using Caterpillar payload systems for a cycle. The system needs to be calibrated for this measurement to function properly.

Estimated Efficiency

Estimated payload per unit of fuel burned for an asset.

Measured Efficiency

Measured payload per unit of fuel burned for an asset.

Productive Efficiency

Summation of total payload with fuel ÷ total fuel with payload burned for productive cycles only.

Total Efficiency

Summation of total payload ÷ total fuel burned.

Total Working Time

• Sum of working time and productive idling for the selected date range.

• Displays values for all assets which report working and idle time.

Average Cycle Time

Typical cycle duration for all cycles in the site of previous week per day.

Fuel Burn Rate

Total fuel consumed ÷ Total duration in hours.

Cost/Cycle

Total cost incurred ÷ Total number of cycles.

CO2 Emitted

Refer to CO2 Emitted to know more.