Create Zones

Zones represent sectioned area(s) within your site where specific functions take place. This can include areas where your assets dump material, pick up material, etc. 

Use zones to improve logic. With Create Zones, you can draw and mark out different zones for a site in map view. The zones available are:

  • Cut/Load

  • Fill/Dump

  • Stockpile

  • Exemption

  • Site Boundary


Refer to Types of Zones for more information on the functionality of each zone type.

Also, identify the number of events that occurred in each zones, and when events (cut/fill, idle time) are tied to the created zones. You can view zone information on Site Summary Fleet View, map view and on Insights Map.

Use these zones to help you create of cycles based on load and dump events and improve overall accuracy of the asset's performance.


Here, you can only create zones for load and dump events of Advanced Productivity- and Load-and Cycle-subscribed assets.

Zones

To create zones for your site:

  1. In Create Zones wizard, click Create Zone drop-down  and select any one of the following:

    • Draw

    • Import  

  • To draw the zone:

    1. Select Draw   and select the zone type from the expanded menu.


      The selection of zone type helps in generating cycles.

    2. Draw the zone in free form shape with a minimum of three points. Click the same start and end points to complete the shape.

    3. This displays the Create Zone pane on the left side, once the zone is drawn.

  • To  import  the zones:

    1. Click Import  . The Import Zone pane is displayed on the left side.

    2. Set the preferred Zone View Limit to locate zones within the specified radius from the site’s pin location. The default Zone View Limit is 5 mile radius.

    3. You can also search zones by its name.

    4. Select from the list of available zones that are alphabetically grouped along with the number of zones.

      • Click Add Zone  to add the respective zone to the site.
      • Click Previewto view the respective zone on the map.
  1. In the Create Zone/Edit Zone pane, enter zone Name in the respective field.


    • When you create zones, ensure the following:
            ◦ Zones don't overlap or intersect.
            ◦ Zones have a minimum of three points while drawing.
            ◦ You only draw a single site boundary around the created zones.
    • Zone names are case-insensitive and allow for spaces. If any of the required criteria isn’t met while entering the zone name, then it will be highlighted in red.


    When adding zone values, use different symbols other than a hyphen (_ & *) or add text to the numbers, such as Area3-7 and Dump4-5. Otherwise, when downloading the data as a .csv file, hyphenated numbers such as 3-7, 4-5 are displayed in date format (3-7 becomes July 3).

  2. This displays the Create Zone pane on the left side, once the zone is drawn.

  3. Change the zone type in the slider pane, in case the incorrect type of zone was created.

  4. Select Color from drop-down list to select your preferred color for the zone and mark it out for easier viewing.

  5. Click Save to check out the created zone within the map.

  6. Once you create the zones, this updates the available zones in the zones section under the slider pane.


    • The created zones are listed under each zone type. Each zone can be selected or deselected to update the zones on the map.
    • If the Site Boundary zone type is created on the map, then the toggle button is auto-enabled.
    • If there are any deleted zone on the map, then the toggle button is auto-enabled.

  7. Select more options  next to the created zone to edit or delete the zone.


    The selected zone is highlighted with a thick border.

    • Click Edit. This displays Edit Zone.

      • Move the plotted end points and replot to create zones.

      • Rename, change zone type or modify zone color, if needed.

      • Click Update.

    • Click Delete. This displays Delete <Zone Type> Zone?. Click Delete to proceed.

  8. Click Next to continue to Add Shifts.

 

Events

On Create Zones, you can also view events (production, idling, etc.) for your assets. To view events:

  1. Select Events from slider  .

  2. On the Select Asset drop down, select from the assets added in Add Assets. The assets are arranged under their respective asset tag drop down lists.


    You can select only one asset at a time.                                                                                                                                       


    You can also the search bar to quickly find any relevant asset by its ID or serial number.                                                    

  3. This displays all events performed by that particular asset. The events are further classified into:

    • Production Events: Includes all segments like load, dump, haul, etc.

    • Idling Events: Includes events like loaded stopped.


    • Events data displays based on how long the asset was operational for. This is indicated by the date range above.
    • Click check to toggle on/off a particular event, making it easier to focus on what matters.

  4. Click Next to continue to Add Shifts.

 

Map Icons and Corresponding Functions

The following table represents icons and their functions found within the map view:

Items

Features

Description

Zoom In

Zoom in the map for viewing the desired asset’s load and dump events.

Zoom Out

Zoom out the map for viewing all the available asset’s load and dump events.

Satellite View the map in Satellite mode.
Terrain View the map in terrain mode.
Recenter

Focus back on the selected location after panning

the map.

Double Up Arrow View the legend events on the map.
Full Screen Expand the entire screen of the map.
Measure Distance

Draw lines on the map for measuring distance and area. Connect lines through points to draw polygons on the map.


• Displays following measure distance pop-up on the map when clicked on.
• Displays the auto-calculated distance and area for the traced path on the map and measure distance pop-up.
• Complete the drawn line by double-clicking on the plotted point. Delete the same single-clicking on the specific point.
• Stop measuring distance by clicking the closed icon of the measure distance pop-up.