Unique VisionLink Productivity Issues
-
PerformancePro Asset Without Payload or Third-Party Assets: Utilizes Target Payload, if available, from the site configuration.
-
PerformancePro Asset With Cat Payload**: Utilizes the aggregated payload data from the asset to provide average payload per cycle.
-
Advanced Productivity Asset Without Payload: Utilizes the target payload if configured.
-
Advanced Productivity Asset With Payload**: Utilizes the cycle payload information from the asset for totals and averages.
• Payload accuracy is determined by onboard payload system, calibration and maintaining the payload system.
• VisionLink Productivity utilizes onboard payload as the primary payload data source. If multiple values are available, the best available value will be utilized.
• For Hauler - Load and Haul and Scrapers specifically, if there is no onboard payload, the Target Payload entered will be utilized.
• You can enter and modify the Target Payload when configuring assets during site creation.
-
Loader – Load & Haul: shows loading cycles not loading events (multiple loading events to fill truck = 1 loading cycle)
-
Load Out: shows individual loading events of the loader
When a asset is parked overnight it will go to Key On - Engine Off as the is currently the only available cycle segment when the engine is not running.
-
Do not kill an asset with disconnect before key switch.
-
Do not shut off asset disconnect immediately after key off before Cat Telematics can upload data (~five minutes) so site reports are sent.
Refer to the Cat Operator and Maintenance Manual for more information. -
Move asset to exemption zone rather than load or dump zone to avoid incorrect segments.
Location information for these events are not shown and these are aggregated every cycle.
Dump times will show zero seconds.
Insights will show empty stopped time or loaded stopped time.
For more information on dump location, refer to Site Summary Utilization and Insights Utilization dashboards.
Why do site KPIs differ on the Sites Dashboard?Why do site KPIs differ on the Sites Dashboard?
KPIs are based on hierarchy of haulers, scraper, and load out.
Payload per hour includes estimated values if payload systems are not installed.
If you’re an E-Customer, you won’t be able to request for an upgrade to Standard or Admin user roles. Your dealer admin can upgrade you as Admin by mapping your CWS ID to the respective account (CCID).