Grade Control Systems

With Grade Control Systems, the attached EC520 Grade Control Devices (GCDs) allow you to connect to the Cat Grade Web Interface on your asset to troubleshoot and change settings, track device details and locate your asset.

View calibration or design files uploaded to the application and ensure they match files uploaded to specific assets on the site. This helps you remotely verify if the correct files are on the asset.

To access this page, navigate to Manage  > Grade Control Systems.


• Refer to Supported File Types to learn more about what files you can upload to access grade-related data.
• Refer to Tag Files to learn more about what all is needed to view and track Map (Insights) details for grade assets.
         ◦ Tag files created with Universal Total Station (UTS) and Real-time Kinematics (RTK) differential GNSS techniques are supported.
• VisionLink Productivity features availability depends on the Cloud Service selected on the machine.
         ◦ If the machine uses VisionLink as the Cloud Service, the supported features include Remote Access, Status Message, Zsnap, File Transfer and Tag File - Productivity Data.

  1. Search: Find an asset or a grade device along with its respective details by its model or serial number. Enter a minimum of three characters to auto-populate search results which will be highlighted in yellow.

  2. Refresh: Click to reload the page and display the latest remote access status, asset details and GCD updates.

  3. Filters  : Narrow the displayed data by the following criteria:

    Click Filters  to do the following:

    • Site

    • Remote Access

    • Grade Control Device

    1. Search for or select the corresponding drop-down to view the required filters.


      For certain filter categories, there are many more options than what’s shown. Click Show All to view them all. From there you can select as many as you like and click Save & Proceed to add them as filters.
      View ImageView Image

    2. Check the interested filters and click Apply.

    3. The filters display as chips next to the date range.

    4. Click close  to remove the filter chip(s).

    5. Alternatively, return to Filters and select Clear All to remove all checked filters.

  4. Pair Device  : Click to pair your asset serial number with a GCD serial number. This is only applicable for assets subscribed to Performance or PerformancePro.

  5. Drop-down View: Expand the drop-down to view all GCDs linked to the respective asset. Select any device in the drop-down table to view details like device name, model number, serial number and firmware.


    • Each linked GCD displays its firmware version and helps you track whether any version is outdated.
    • In case of outdated firmware, refer to Grade SIS Documents to understand the compatibility of each version with the respective asset types. You can also contact your dealer, citing the above documents for quicker resolution.
             ◦ You can find devices moved onto a different asset by their serial number and model.

  6. Asset Status: An indicator is displayed near each asset to convey the following:

    •  : Asset is keyed on.

    •  : Asset is keyed off.

    •  : No status reported from the asset.

    •  : Asset status is not supported

  7. Remote Access Status: Indicates the following status of the asset-GCD pairing:

    • Online  : Shows that the asset is paired with the GCD and has one of the following operators display models, which can be remotely accessed: 

      • TD520

      • TD540

      • EC520

    Even if one of the two devices mentioned is available, the status shows as Online. 


    • When an asset shows as Online, the status also indicates whether none, one or both remote access devices (TD5XX display and EC520) are available.
    • There may be a delay of up to 10 minutes before GCD displays Online after an asset key is turned on.

    1. Click Online  .

      • Remote Access pop-up opens and displays the following:

        • Grade Control Display


          The Grade Control Display option is enabled only for assets equipped with a compatible and supported operator display.

        1. Select the Grade Control Display option that redirects to the TD5XX operator display interface.

        2. Give it few seconds while the remote connection is established.

        3. Once the operator accepts the remote-control request. You can do the following:

          • Open, close and switch between screens and menus.

          • Access workflow pages, configuration panels and settings pages.

          • View all operator-visible information such as task details, cut/fill values, warnings and system status.

          • Tap, drag, scroll and perform all standard touch gestures. You can select menu items, open dialog components and modify input fields.

          • Adjust display layers, measurement values or map-related settings (as permitted by the system).


            • To access Grade Control Display remote service, ensure that the GCD software version is v2.25 or higher. To know more, refer to SIS . 
            ◦ The ScreenViewer will automatically install a TD540 display when updating to v2.25 or higher.
            1) After the installation, the ScreenViewer must be opened on the display to perform the initial remote access registration.
            2) Upon first remote connection, the user should select the Do not show again checkbox and allow the app access.
            3) See SIS media M0168943 for more detailed instructions for onboard configuration.

            • Only one active control mode session is allowed at any time.
            • Anyone additionally joining in from a remote system will join in View Only mode. 
            • The control mode request times out if not accepted within 60 seconds.
            • If the operator rejects control or the session times out, the system automatically returns to View Only mode.  

        • Grade Web Interface

        1. Select this to be taken to the Cat Grade Web Interface login for the selected asset in a new tab.

        2. Enter the login credentials created upon the initial setup of the onboard grade system.


          • For software version 2.23, a login is not required for standard operation. Credentials are needed only when unlocking the system to make configuration changes. 
          • To access Grade Web Interface remote service, ensure that the Grade Web Interface software version is v2.16 or higher. To know more, refer to Grade SIS Documents .
          • While you can delete .pnt (recorded point) files synced from an asset to a site on the application, the file remains on the asset. You can access the asset remotely to delete the file from there.    
          • To know more, refer to SIS  > enter your asset serial number and grade-specific SOTTA (System Operations, Troubleshooting, Test & Adjust) details. Learn how to verify design, calibration and other files on the Cat Grade Web Interface.

    • Offline  : Shows that none of the grade control devices are currently available for Remote Access. This can occur when:

      • The asset is switched off/keyed off. 

      • The system is unable to determine the asset’s status due to connectivity.


      If the device is offline, the connection request won’t proceed.

    • Not Supported  : Shows that the asset is paired with the GCD but the GCD doesn’t support remote access capability.

    • Unavailable (Pairing Failed)  :  Shows that the asset isn't paired with the GCD.

  8. Table View: View and track all the following details relevant to your asset-GCD pairing:

    Column Name

    Definition

    Assets

    Lists assets with their ID and serial number. The folloiwng assets display:

    • Assets paired to GCDs (with either factory-installed or after-factory-installed network manager based-EC520).
    • Assets manually paired to EC520 GCDs.                      
    • Assets that failed to pair with a GCD.                           
    Last Reported Shows the date, timestamp and time zone of the asset's last reported data based on data fetched from the Grade Control System Status Message.
    Note: This is applicable only for the EC520 Grade Control System device and last reported details will not be displayed for CB460 Grade Control System device. 
    Site(s)

    Displays all the sites where the asset operates.

    Onboard Devices

    Lists the GCD serial number and type paired with the particular asset.

    In case any errors occurred during pairing, you can view the exact error description as well.
    View ImageView Image

  9. More Options  : Find the following options next to your asset of interest once you pair an asset with a GCD:


    The options available will vary based on which kind of EC520 GCD [Unified Cloud Management-enabled (UCM) or not] is paired with the asset.

    • Locate Asset: View map location of the site where the asset was last reported.

    • Download Snapshot: Save snapshot (.zsnap) files to help with onboard system troubleshooting.

    • Device Details: View your asset and device details (including comms., radio, sensors, display and more), updated in real time.

  10. Show (rows): Choose between 20, 40, 60 and 80 table rows to be displayed at a glance.

 

Supported Grade Subscription Configurations

Grade subscriptions must include one of the following add-on configurations to enable supported features and compatibility:

Subscription Configuration

EC520 Grade Control Device (GCD) Capabilities

Performance + Grade Connectivity

• GCD Pairing

• Support transferring of file types [for example, design (.dsz), screenshots (.zsnap) and recorded points (.pnt), etc.]

• Grade device detail

• Grade corrections over the air

• Remote access status

 

PerformancePro + 3D Productivity

Includes all capabilities available in Performance + Grade Connectivity, plus Process Tag File and 3D Visualization.