Files

With Files, you can perform the following:

  • Upload files of different categories (design, survey, geodata, etc. ) to your site and its assets.

  • Manage uploaded files, including syncing to assets, downloading, copying and more.

  • Download files into a format that can be copied to a USB device and transferred to an asset.

Files helps you achieve the following benefits:

  • The Map (Insights) data visualizes the latest site images. This adds layers of data to quantify and measure work done and remaining.

  • Your site’s assets synced with the latest site design and calibration files through the cloud rather than manual transfer.

  • Site monitoring is enhanced and easier than before, with vertical accuracy measured as well. 

  • Stored files for easy access and retrieval across others in your team using VisionLink Productivity. 

Navigate to Manage > Files to get started.

 

Supported File Types

To view grade-related data on Site Summary map view and Map (Insights), uploading files of certain file type to your site is necessary. Calibration and design files help you generate .tag files.

These file types are as follows:

Category

File Type

File Size Limit Asset Tag Visibility

Use Case

Onboard

Offboard

Notes

Avoidance Zone

.avoid.svl (avoidance zone file)

50MB (max.) Grade
Compact
Map (Insights) Used to define specific areas on a site that assets should avoid. 

Optional

Optional

• Upload a valid calibration file before adding avoidance zone file.

• File must include at least one closed and not more than 800 polygon edges.

• Only one avoidance zone file is allowed per site at a time.

Calibration

.cal (calibration file)

No limit

Grade

Compact

Grade & Compact

Map (Insights)

Used to convert global latitude/longitude values to northing/easting distance grid values.

Required

Required

• You need to upload a calibration file before uploading any design or geodata files.

• You can sync calibration files from the application to your site's assets.

• The minimum requirement to view Measured Volume KPI > View Completed data is a site with boundary and calibration (.cal or .dc) files.

.dc (older used by Trimble controllers; includes Point Pair details)

Design

.dsz (design file)

Less than 25MB (recomm.)

50MB (max.)

Grade

Compact

Grade & Compact

Map (Insights)

Used to calculate Work Remaining (volume left to be moved to achieve the target elevation) and send to the asset to set the target elevation.

Optional

Optional

• It is recommended to upload all design files lesser than 25MB to avoid complications in data processing.

• .vcl and .xml files will only be supported for assets with EC520 grade control devices (GCDs) when the application prepares files for USB Download.

• You can sync design files from the application to your site's assets.

• A design file is required to view Measured Volume KPI > View Remaining data. You can set and change the default design file you view on Site Summary and Insights.

• The application automatically extracts .dsz files into the following:

° .svd (design): View this file on Site Summary Production map view and Map (Insights) when selecting Work Remaining.

° .svl (linework): View the design file's lineworks on Site Summary Production map view and Map (Insights) on top of any selected layer (zones, events, elevation, etc.).

• Any .xml file not named “CoordSystemDatabase.xml” will be considered under the Design category. You can modify this before uploading the file. If it’s named so, you can only upload it as a geodata file.

.vcl (proprietary Trimble-format machine design file with multiple layers)

Used to support Cat Grade system availed on the site's grade assets.

.xml (landXML design file))

Used to store civil/survey work data in a text format for easy retrieval.

.ttm (office design file)

Used to monitor projects and operations.

Geodata

.ggf (geoid file)

No limit

NA

Map (Insights)

Used to support site calibration (if needed).

Required

Required

NA

.sgf (shift grid file)

.dat (snake grid file)

.dgf (GPS Pathfinder Office-geoid grid file)

.xml (specifically CoordSystemDatabase.xml file used in conjunction with calibration and other geodata files)

When uploading geodata files, only CoordSystemDatabase.xml files are supported. For other .xml (like LandXML) files, upload as a design file.

Image

.tiff/.tif (geotiff file)

5MB (min.)

80GB (max.)

NA

Site Summary map view

Used to add site layers to the existing map view.

NA

Required

• You can copy processed site image files from one site to another.

• You cannot select a default site image. The last uploaded image is set as the default.

• You cannot upload an image to multiple sites. Re-upload the same image wherever necessary.

Survey

.ttm (survey surface file)

No limit

Grade

Compact

Grade & Compact

Map (Insights)

Used for construction work on a surface and to visualize volume calculation data.

NA

Optional

NA

Recorded Point

.pnt  (recorded point location file)

No limit

Grade

Compact

Grade & Compact

Map (Insights)

Used as part of a work order created by operator to store latest depth point reached by an asset.

NA

Optional

• You can view these files (automatically synced from the site’s assets) and only Download or Delete them.

• Each .pnt file displays with the details (asset ID, serial number, make and model) of the asset that recorded it.

• In some cases, the asset syncing the file will no longer be a part of the site. If so, past .pnt file versions will still be present in the site. Future versions, however, from the same asset won’t be available.
• While you can delete .pnt (recorded point) files synced from an asset to a site on the application, the file remains on the asset. You can access the asset remotely to delete the file from there.