Copy Jobsite
Quickly create multiple jobsites by copying existing ones with the Copy option in more options list.
It helps:
- Split up operations for larger jobsites,
- Track assets that perform multiple activities in a single jobsite easily and
- Carry over settings and preferences into new jobsites, saving time and effort.
To copy a jobsite:
1. Visit Jobsites Dashboard and find the jobsite you want to copy.
2. Whether in Grid, List or Map View, click more options icon. Select Copy.
3. This opens the Copy Site page.
4. Ensure that the site name is changed to distinguish from the existing site.
5. Make any desired changes within the Add Site Details, Add Assets, Create Zones and Add Shifts steps as well.
Refer to Create Site to learn more about setting up sites and the steps involved.
6. Review site details and click Finish in the Review Site step to create site.
You can find and view copied jobsites as the first card in Jobsites Dashboard.